Hi,
My customer seems to be having an issue similar to this one, but looks like they stopped responding so there wasn't a resolution.

Inquiry from the customer-
Please find our charging circuit as below. Per our design, Iset is set to ~415mA.
If the Vin is 5V or lower than 5V, when the charging current tapers to around 50mA (~10% of Iset), the CHG terminal will turns to high and the charging current will drops to below 10mA.
But, I found that if the Vin is higher than 5V, the termination current would become higher than 10% of Iset. And, the charging current would not stop and continue to charge the battery until the battery enters over-charge protection (4.25V). Please find my findings as below table.
|
Vin |
termination current |
Charging current after CHG terminal turn to high |
|
5.0V |
~50mA |
<10mA |
|
5.1V |
~60mA |
From ~40mA to ~20mA |
|
5.3V |
~240mA |
From ~220mAto ~150mA |
- Is it the expected result? The maximum Vin should be 6.5V. I don’t know why the termination current will be changed by the Vin and the charging current cannot terminate.
- Can I stop the charging current or only keep the charging current under 10mA, after CHG terminal turn to high (Condition: any Vin is under Max Vin)?
- Can I keep the termination current close to 10% of Iset (Condition: any Vin is under Max Vin)?
Our charging circuit: