This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Recommended component values of TPS51396

Other Parts Discussed in Thread: TPS51396, TPS568230

Hi team,

I have 2 questions for TPS51396 datasheet description.

1. Where is CFF cap in EVM schematic? And what is its function?

2. Do we have recommended component value for Vout=1.8V?

Best regards,

Hardy

  • Hi Hardy,

    1. The feedforward capacitor, which is a cap placed across the high side feedback resistor, can improve the stability and bandwidth of a power supply. This capacitor adds a zero and a pole to the control loop, which can be strategically placed to improve the phase margin and bandwidth. Details can be checked the linked app note.

    https://www.ti.com/lit/an/slva466a/slva466a.pdf

    2. For 1.8Vout, you can use 1.2uH inductor, Rlow=30K, Rup=60K resistor. Others can be same with 1Vout. Honestly, you can also use TPS568230 Webench to select external components.

    Thanks,

    Lishuang