Hi Sir,
I used the BQ40z50-R2 in our battery pack.
From the page 13 of BQ40z50-R2 datasheet , the internal pullup resistance (Rntc(pu)) min value is 14.4Kohm, type value is 18Kohm, Max Value is 21.6Kohm.
But for the NTC Coefficient a1~a5, b1~b4, in the calculation table, the R_TH type value is 18Kohm , but the Resistor tolerance is ±1%,there is no reference to the datasheet for 20% accuracy.
I want to know, what is the accuracy of the R_TNC(PU) resistor?
Thanks ,
Billy