This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8860-Q1: VDDIO/EN pin internal Pull Up resistor or current source

Part Number: LP8860-Q1

I drive LP8860Q1 VDDIO/EN pin through a 10K series resistor. I found that if my control line is at 0V, then VDDIO/EN pin is at 2.48V (I use VDD = 3.0V).

This tells me that VDDIO/EN pin has an internal Pull Up resistor of about 2K in value.  Part spec sheet says nothing about this internal PU or a current source on VDDIO/EN pin. Please let me know if LP8860 par needs an errata to outline this design difference.