Hello,
I was wondering around what value the optional capacitors in the matching circuit should be? A simple question I'm sure.
Thanks,
Chris
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I was wondering around what value the optional capacitors in the matching circuit should be? A simple question I'm sure.
Thanks,
Chris
Hello Chris,
Using my best conservative design practice, I would use 10uF ceramic caps for the input and output capacitors. I would use a 10nF ceramic capacitor for the noise reduction capacitor, Cnr. And, if I were using the adjustable version of the LDO and decided to use a 100kohm resistor for the R1 (top) feedback resistor then I would use a 1nF ceramic feedback capacitor (Fig 32).
Bill