Other Parts Discussed in Thread: BQ25155, BQ25505
Hello,
one of my customers is starting a BMS project where they need some advice.
- Li-Ion Cells (one or more in paralel, only one in series - 3.7V)
- The lion cell has no protection circuitry. Is a protection circuit needed when the battery is permanently installed?
- charging takes place through a small solar cell (additionally via USB)
- low power consumption
- precise detection of battery fuel status, best case with additional consideration of self-discharge, aging
- small Layout and cheap
Which components would you recommend to cover the main functions? Which optional components would you suggest?
Thanks,
Alen