This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24078: bq24078

Part Number: BQ24078
Other Parts Discussed in Thread: BQ24072, BQ24073

Hi Sir,

My customer will use bq24078 for 4.2V battery, what means TD as below?

Do you have reference schematic for share?

Thanks, Ian.

  • Hi Ian,

    The TD functionality on the BQ24072 and BQ24073 devices refers to the pin that is available on those devices but not the others. It gives the user the option to disable termination. The configuration for devices with a TD pin is the same with the TD pin being pulled high to disable charger termination or to VSS to enable charge termination. Note: this pin will only be checked at startup.