Other Parts Discussed in Thread: LM5145
Hi Team,
Our customer is trying to simulate the LM5117 with Vin=47V and Vout=44V, Iout=6A.
In pspice simulation, they can't reach the output voltage of 44V because min. tHO(OFF) is around 1us. Vout is around 40V.
RT is set to 42k2 for 120 kHz.
According to the datasheet, it should be possible to reach 44V. Duty cycle = 44/47 = 0,936 should be possible at 120 kHz.
They have already checked the current signal on Rs and RAMP. Everything seems ok.
They using an inductor of 47µH.
If the Vin increases to 55V in the simulation, it works.
Is there a problem with the pspice model? Is it possible to reach a duty cycle of 0,936 at 120 kHz.
Please let me know your comment.
Thanks,
Jonathan