This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24703: ESD information

Part Number: BQ24703

Hello Team,

My customer is looking for the ESD information for the BQ24703 device, can you share with us the CDM and HBM rating?

Regards,

REnan

  • Hi Renan,

    The HBM is 2000 V, and the CDM is 750 V.

    Is this for a new project? The BQ24703 is a legacy device. TI's newer chargers can provide many benefits, including higher efficiency, higher integration, lower BOM count, and more features. If you send me the design requirements, then I can help suggest a charger which would fit your application best.

    Best regards,

    Angelo