This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61196: Can TPS61196 reach 400mA?

Part Number: TPS61196


Hi,

Can TPS61196 reach 400mA and meet the following SPEC?

INPUT=24VDC

OUTPUT= 36V/400mA * 6 ch LED(Need current balance )

Must have dimming(45ms on/45 ms off)

When the Driver is abnormal need the pin to send an error signal  (ex.OVP.OTP.OCP.OPEN...)

total power 86.4W

regards

Rock