Hello TI,
We are working on BQ24773, Observing issues in ACOK voltage
1. At 99% (Monitor by using BQ27542) of battery charging state, ACOK voltage is drop to 3V (which require 3.3V to continue charging)
2. Because of ACOK changes, ACDET also change 2.9V to 2.846V (As per the observation) it's because of Input adaptor voltage change to 5V to 4.8V
3. Whos affecting on ACOK voltage, how to stable the ACOK (Problem is observe at 99% of SOC otherwise there was no any variation in ACOK voltage)
4. Also test with different pull-up resistor across the ACOK pin (10k and 4.7k), but there was no any change
5. Because of this issues battery is not going charge 100%, Full battery capacity is 13200 and charging stop at 12900 nearby
6. at BQ27542 also observe that there was drastic changes cycle count, when i start one cycle with zero cycle count after completing one cycle cycle count goes to 32
how to resolve the issues or there was any related documents to understand and work on it stable down system
Thanks,
Rahul