Hi, All
How can I write setting parameter into TPS65070, in I2C bus TPS65070 is a slave who is the master DSP,ARM or MCU?? For example ARM is the master, But in power-on stage ARM has not booted. Anybody know how can I do it??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have discussed with some friends about this question, and we think we need a other MCU to communicate with TPS65070, this MCU storged TPS65070 setting parameter and when system power on, first MCU init and configer TPS65070,second TPS65070 power on, Third Application Processor boot. In this way we need add other MCU to be a power management IC, It seems not a good idea for E-BOM cost control.
Anybody has good suggestion??
What are you trying to achieve by programming through I2C? If start-up sequencing, I recommend using one of the TPS6507xx variants which provide preprogrammed internal sequencing to power up the processor. Once the processor is powered up, it can issue I2C commands to the TPS6507xx.
Based on your duplicate post: http://e2e.ti.com/support/dsp/sitara_arm174_microprocessors/f/47/p/96939/341821.aspx#341821
I recommend the TPS65070 which is by default, setup for the OMAP-L138 per table 9 and figures 49 and 50 in the datasheet.