This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR16006: Minimum & maximum limits of "Ishdn" & "Ishdn_hyst

Part Number: LMR16006


Dear sir/Madam,

We used "/SHDN" to adjust the system turn on voltage by using external resistors. According to the datasheet Ishdn = 1µA & Ishdn_hyst = 3.2µA @Tj=25°C.

The problem is that the datasheet doesn't give the minimum & maximum limits of these values. Therefore we cannot determine the turn on voltage and the hysteresis when the temperature varies between -40°C and +125°C!

Could you give us the minimum & maximum limits of "Ishdn" & "Ishdn_hyst" ?

 Sincerely,