Hi,
I am looking for 12V,2/1.5A constant output.
My input voltage is 10.7V ,which is driven by a 3S1P battery pack.
Can you suggest suitable boost IC for my application.
Can I use LM2623?
Thanks
Kiran
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kiran,
I would suggest a buck-boost converter such as TPS55288,
or a sepic topology using LM5155, or LM5157 if the output current is 1.5A.