This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61372: Powering board on no load

Part Number: TPS61372

Can we power the board on no load?

Designed for max current: 30mA

Output : 6.5V

Input : 3.3V