This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61236P: Slow start up takes 35 seconds to reach 5V

Part Number: TPS61236P
Other Parts Discussed in Thread: BQ24773

Above is a scope of the startup of boost based on the TPS61236P.  the circuit quickly rises to the  input voltage. Hangs there about 8 seconds and then slowly begins to rise to the 5V output.  This circuit is being feed off the Sys output voltage of a bq24773 battery charger chip.  The battery charger is not charging while we are booting.  I am running solely off battery.

The 5V output has the following capacitors attached.

 

1 10uF

1 4.7uF

3 22uF

1 47uF

 

C total  127.7uF

the 5V power supply input comes off the sys power output from the battery charger.  Schematics can sent in private message.