Hello,
I would appreciate any feedback regarding customer question below:
Device: LP8869QPWPRQ1
The above IC can be used with SEPICs, so is it correct to think that buck-boost operation is possible as well?
For reference, the conditions which the customer is expecting to use this device is below:
Red:7 series x 3 parallel, green: 7 series x 3 parallel, blue:7 series x 3 parallel
Using one device for each color. (1ch is used in 1 parallel)
Considering input voltage 24V, and output in the range of 15V to 28V depending on the color.
Expecting maximum current per channel to be 50mA.