Part Number: BQ24073
Hi,
-5V input stage current consumption: 0.137A at 5V
-BQ24073 IC's CC measured value: 0.12A at 3.7V,
When the battery is in 3.7V condition, the output voltage of the charger IC is 4.2V.
Therefore, the overall charging efficiency of the board is calculated as (4.2V*0.12A)/(5V*0.137A)*100 = 73.57%.
(0.137A of input terminal is the value including charging current and system consumption current.)
If the above is not abnormal,
I want to know how much power bank battery capacity is needed when I want to charge the cradle with 300mA battery once using the power bank.
Assuming that the output efficiency of the 5V stage through the power bank boost ic is 90%.
[case 1]
Cradle battery power: 3.7V * 0.3A = 1.11W.
The efficiency to charge 1.11W is 73.57%, so 1.508W is required on the cradle side.
In order to output 1.508W from the power bank, 90% efficiency is generated,
so 1.675W must be supplied from the power bank battery and
1.675W / 3.7V = 452.7mA battery capacity is required.
In other words, 452.7mA of battery capacity is required in Power Bank to charge Cradle's 300mA battery once.
(Overall efficiency: 300mA/452.7mA=66.2%)
[case 2]
Cradle battery power: 3.7V * 0.3A = 1.11W.
However, 4.2V is output from the charger IC when the battery is output, so 4.2V *0.3A = 1.26W is required.
73.57% efficiency is generated to charge 1.26W, so 1.712W is required on the cradle side.
In order to output 1.7121W from the power bank, 90% efficiency is generated,
so 1.902W must be supplied from the power bank battery, and 1.902W / 3.7V = 514mA battery capacity is required.
In other words, 514mA of battery capacity is required in Power Bank to charge Cradle's 300mA battery once.
(Total efficiency: 300mA/514Ma=58.3%)
Which of the above two efficiency calculation methods(case 1, 2) is calculated correctly?
If the calculation method is not correct, please tell me how to calculate the required power bank capacity to charge a 300mA battery once.
Regards,
MJ