We are developing a 1200W power supply by using your UCC28070A. the power supply adopts bridgeless PFC construction. There are some unstable AC input current at certain AC input condition (85.8Vac, 104.3Vac, 118.2Vac, etc) when apply full load, the worst condition is at around 85.8Vac and full load, but 83Vac and 87Vac condition become normal. When adjust AC input to 104.3Vac and 118.2Vac condition, there is also sudden unstable (<0.5s) but becomes normal immediately. When apply half load, there is no obvious unstable current any more. We see there is around 500us phase difference between AC input voltage and VINAC pin 5 of UCC28070A, not sure this is a problem. Also we set around 200us dead time (disable PFC gate driver) at AC zero-crossing duration, not sure this is the cause to the problem. Attached file show the schematic diagram and related waveforms, please help to study. Thanks in advance!AC21302LF PFC UCC28070 schematic and waveform comparison.xls