Hi,
I had a device which stopped chraging at 94% batt level (average current = 0, remaining capacity = 2122, full charge capacity = 2258 ).
I sent a 'soft reset' (0x0042) to the device - and battery level changed immediatly to 99% (average current = 0, remaining capacity = 2420, full charge capacity = 2445 ).
Can you please explain the fuel gauge process during the soft reset cycle, that cuased those values to change?
Which of those values sets should I consider accurate?
Thanks,
Yaron