Other Parts Discussed in Thread: LM76202-Q1
I am not sure how to interpret the data given in the data sheet under absolute maximum ratings:
I have 24 V Output and have to survive negative surges. What is the maximum negative voltage I must not exceed at the IN Pin?
under Absolute maximum ratings:
IN, IN-OUT | -42 | 42 V
IN, IN-OUT (350ms transient) | -55 | 55 V
Now do I have to subtract the 24 V Out Voltage for the negative voltage limit like this? In-Out = Limit (In-24V=-42); In = -18V ?
Wich is less than given under recommended operation where there is not the addition of IN-OUT:
IN | -40 | 40 | V
I appreciate your help. Many thanks in advance
Joel