This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27426: wrong full capacity estimation

Part Number: BQ27426
Other Parts Discussed in Thread: GPCCHEM, BQSTUDIO

Hi,

I am using BQ27426 with chem ID 0x1202 (4.2V), Initializatizing 'Design Capacity' to 2600 mAh.

I have encountered a situation where the fuel gauge estimates the full charge capacity as 2983 (and still  battery level is at 80%).

the scenario in which this issue happend was:

1. Charge the device to 50%

2. Power off the device for 2 days (FG still connected to battery)

3. Charge the device till charging stops - at this statge the full capacity goes up from 2500 to 2893).

I attach an xls file with fuel gauge readings during this process.

How can this be explained?

Are there any parameters that can cuase this kind of behavior?

Thanks,

Yaron