Hi Team,
The TPS22945 datasheet states that "OC is an open-drain MOSFET and requires a pullup resistor between VIN and OC". Can I pull-up the device to a rail other than VIN? For example, use the LS for a 5V application and pull-up OC to a separate 3.3V? It looks like it would be possible, but I just want to make sure there are no potential issues such as ESD diodes clamping OC to VIN (conducting if the 3.3V ramps before the 5V VIN).
Thanks,
Antonio