Hello,
The datasheet does not specify the lowest limit for the current settings. It contains just 3 examples.
My circuit utilizes TPS2590 with the following parameters:
- Vin = 8V
- Cout = 2.2uF
- DC load = 150 R
- RRFLT = 500K ( I= 0.4A)
- RLIM = 250K (I= 0.8A)
Normally load takes just 53mA (8V/150R), but in fault condition it may be short; so the TPS2590 is used just as a protection circuit. Is it going to work reliably with such low normal current and the fault current threshold of 0.4A that is less than 1A example in the datasheet?
Thanks,
Vlad