This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM51551: Webench simulation issue

Part Number: LM51551

Dear Team,

I have entered the below listed criterias into Webench to get a solution offer:

Vin: 24V */-5%

Vout: 30V

Iout: 4A

Although the a solution with LM51551 is one of the solutions listed, the system returns an error message when I try to make a simulation with default component values. Changing the values does not change the status.

Could you please check the Webench model for this device?

Best Regards,

Caglar