This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS43061: TPS43061 consumes large current on wakeup

Part Number: TPS43061

In the latest batch we've noticed that some TPS43061 devices on wake-up consume large currents from the VIN pin and do not functioning properly. The failure is intermittent (happens after multiple tries) and even when happens, the device eventually wakes up after a few seconds. When the failure does occur these are the symptoms that we see:
1. Large current consumption into VIN pin (>100mA)
2. EN pin remains low (internal pull-up not engaging)
3. VCC pin goes high immediately with VIN (normally the internal LDO should be disabled while EN is low)
4. SS remains low
5. HDRV pin goes high (to the same voltage as VIN)
Replacing the TPS43061 on one of the failing boards solved the problem. We would like to understand if this failure could have been caused by improper handling at the manufacturing facility, or whether there is another explanation to the failure.
Thank you