Other Parts Discussed in Thread: TPS23523,
Would this part survive the following during surge testing-
8/20 uS for differential mode surge +/- 1kV 2ohm and common mode surge +/- 2kV 12 ohm surge?
Thanks,
Lauren
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Lauren,
TPS23523 is ideal for surge protection. The ORing portion would block reverse current flow during -ve surges.
LM5067 would need additional circuits as shown in Figure 9-11 and in some cases ORing controller at the input to support surges.
Best Regards, Rakesh