This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ77915: BQ77915

Part Number: BQ77915

When low side MOSFETs are OFF, why pack voltage in not zero when pack is open circuit. any suggestions to make output voltage zero when read with multimeter.

  • Hi Gururaj,

    If you want to read zero with a multimeter, you would need to detect that the FET outputs are low and then short the pack terminals together. The device pulls down on CHG when off.

    Best regards,

    Matt

  • Hello Matt,

    You are correct once we short pack terminals voltage is zero. But how a service person will come to know where BMS is in on state or off state. when BMS is inside the battery and packed. Short terminal is not safe options to check status of BMS. Please can you suggest any extra circuit to make output voltage zero when DSG mosfet is off.

  • Maybe applying some type of load to the PACK when making the measurement (like 100k or so) might be helpful for this purpose. I think this will be a common issue for many batteries with protection FETs since PACK- is disconnected from the cells.

    Best regards,

    Matt