Other Parts Discussed in Thread: LM5164
Dear Team,
We have a designed buck with LM5164.
With Vin range 30V-75Vdc (Typical 50V). Vout=0.3Amps Max. Whereas my Load current typical is 0.1A.
to get the max efficiency at light load i am planning to run PMIC at 125KHz.. which results into 330uH.
for the above spec (30Vin-70Vin, 5Vout,0.3Aout) In Webbench its recommonding 2Amps Inductor, and in Excel Calculator Its >1.8A.
as per the datasheet formulae calculation it IL(peak) = 0.3A+0.1A= 0.4A
Pls suggest .. Can i go with 0.6Amps Inductor (MPN EST1060T331MDGA, MAKE- TAIYO YUDEN) ??