Other Parts Discussed in Thread: LM3532, USB2ANY
I've had identical problems as John Connely48 in this thread:
After downloading the LM3532 GUI provided in that thread, I was able to install it and connect to the USB2ANY. However, there was no way to enable the onboard 3.3V, so I had to hook up an external supply.
It seems I'm able to interact with the LM3532. However, when I perform a read (such as read ALS Zone Boundary), after 10 seconds or so, the app quits.
Is there an updated LM3532 GUI app? Is the LM3532 no longer supported?