Part Number: BQ20Z95
Hello TI experts,
my customer is in mass production of battery pack using BQ20Z95 few years ago,
recently they found some problems.
- gauging suddenly falls from 50% to 25%
- cannot wake up after cut off protection (no voltage detection from the pack)
- cannot charge even detect the very low voltage
so could you review the schematic if there is anything wrong?
and i also attach the cell specification for your convenience.
- Samsung SDI ICP544382A (3.85V 2800mAh)
- 3S1P
Please check this issues. Thanks.
Best regards,
Chase