Hi,
I am trying to design AC to DC converter with flyback topology. With input RMS voltage =240V, ouput 24V, 2A. I have used web bench power supply to design this circuit. I have simulated the circuit in TINA but I am not getting desired ouptut. I would like to know the following :
- I would like to know why am I not getting desired output when I have designed the circuit similar to web bench power supply. Is something wrong with Web bench or it is the issue with TINA or my circuit designing? I have used non linear secondary output transformer and editted the total number of windings to suit the requirement. Please let me know what are the changes I will have to make in this circuit to get the desired ouput.
- I have attached my TINA file.
I suspect the reason for faulty output is due to transformer-
Thanks,
Ashok