This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27410-G1: How does it handle constant partly discharges

Part Number: BQ27410-G1

If the battery is never discharged fully (or even below 70%), will that cause the fuelgauge's learned capacity (Full Charge Capacity) to drift over many cycles?

I've have seen from our logs that after a few charge-discharge cycles the state-of-health drops to the order of 85% of normal capacity. I've also seen that the batteries are almost never discharged to below 80% before they are fully charged again.  It is with a 7200mAh lithium-polymer battery.  Current draw is never more than 1.5A and charging is also done at 1.5A.  We are well within the specs of the battery.

regards