Other Parts Discussed in Thread: BQ78350, BQ76200,
Hi;
I have a Costum BMS which consist of bq76200 , bq76940 and bq78350 ICs. My problem is that All FETs are burning while making short circuit test. The problem is occuring when IC tries to exit from recovery mode. In other words, When SC occurs, FETs shut down the output and wait for 5sec ( bq78350 recover time ). After that, while SC condition is still present, FETs are burning(Short) and fuse is blowing.
I have 7 CHG and 7 DSG parelel FETs and CHG/DSG resistors for bq76200 are 100 ohm. The protection level for bq78350 ( ASCD) is in the minumum level. ( 70us, 176 A ).
If you further interest, I can share the Schematic design file.
Thank you.