This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3532: Possible to program the POR (Power On Reset) registers?

Part Number: LM3532

I want to use the LM3532 as a standalone chip. I would preprogram its POR registers so that it refers to those settings on power up.

Is this possible? My tests thus far suggest the POR registers are not being set.

The POR table on 7.6 in the manual: 

https://www.ti.com/lit/ds/symlink/lm3532.pdf