When I don't need all 16 cells of the BQ77216, how should I connect the inputs?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Cell count for the BQ77216 is typically reduced by shorting the inputs starting at the top, see the BQ77216 data sheet figure 9-3 for an example with 14 cells. Cells which are below the VUV_MIN UV Detection Disabled Threshold in the section 7.5 DC Characteristics are not used for UV detection. Shorted cells also will not fault from OV or the open wire detection.
Cell inputs in the center of the stack can be shorted also. Cell 1 has a different open wire detection threshold since it operates at VSS, see the VOW OW Detection Threshold parameter. Shorting cell 1 is not recommended.