Part Number: TPS65150
Hi
My TPS65150 schematic is on the below.
If we don't use the VCOM buffer and derive the VCOM voltage 4V with resistor divider 165K ohm and 95.3K ohm, the 5V input supply current is normal.
If we use the VCOM buffer, the 5V input current would increase 700mA than the above condition.
We follow the design guide in the data sheet and hope for some suggestion.
Thanks!
Wiiliam.