]As far as I understand the BQ34110 will learn over time what the battery is all about.
It learns from discharge/charge cycles to adjust and improve the accuracy of the SOC and other parameters.
In case the battery pack and the BQ34110 are separated from each other (disconnecting the pack and not having the BQ34110 integrated inside the pack) the power of the BQ34110 is removed and information is lost.
Is there a way to preserve all those required parameters/data from the chip so it can be restored and little is lost?
Regards,
Roland