Other Parts Discussed in Thread: BQ76942
Hello, I wish to use a BQ76952 for balancing the cells of a12S battery pack composed of two 6S packs in series. I do not need any monitoring or circuit protection aside from balancing. If I want to use the internal fets, do I need to use any pins aside from the VC pins, Bat, Vss, and REG18? Would the following circuit suffice?