This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5164: Inquiries about UL standard certification

Part Number: LM5164

Hi,

When manufacturing an end-equipment using the following products from a customer,

there was an inquiry about whether it would be a problem in obtaining UL standard certification.

Can there be a problem in obtaining UL standard certification when using the following products?

Part name : LM5164DDAR

In my opinion, UL standard certification does not seem to be a problem because it is an end-equipment.

However, is it possible to check if each of the above products has UL-related certification or if there is a required product?

Is there a way to check if the component has UL certification?

Thanks.

Regards,

MJ