Hi,
When manufacturing an end-equipment using the following products from a customer,
there was an inquiry about whether it would be a problem in obtaining UL standard certification.
Can there be a problem in obtaining UL standard certification when using the following products?
Part name : TPS70933QDBVRQ1
In my opinion, UL standard certification does not seem to be a problem because it is an end-equipment.
However, is it possible to check if each of the above products has UL-related certification or if there is a required product?
Is there a way to check if the component has UL certification?
Thanks.
Regards,
MJ