Hi,
I am developing a 5kW PSFB with UCC28950.
The waveform below is the waveform of main transformer (pink) and the VDS waveform (yellow) of the MOSFET QB(based on the datasheet application)
at 15% of the total load current.
It seems that the visible waveform is valley switching, is it correct?
The load current should be about 50%(load current 100A) until the visible waveform disappears
completely.
It seems like ZVS is going in then.
But the heat of the MOSFET is too hot until then.
Is it right to take the Llk bigger to get the ZVS in earlier?
Currently DELAB is using 15kohm.
Regards,
Kwangwoon.