Dear,
we are using for our project the BQ76930 for a 8S battery and I would have two question about it.
1. From the datasheet I am not clearly sure if I interpret good the requirements
- Under one set (VC1-VC5, VC6-VC10) can be balanced multiple cells but not adjacent. This means (in a 8S scenario) Cell 4 and 5 are allowed even if they are adjacent, but are in different sets?
2. I would have a question regarding he current measurement. The scenario:
If no load is attached the raw 16bit ADC value is 0x004F, with a Rsense of 0.5mOhms this corresponds to about +1.3A. First of all I don't know if this is correct that there would be such a enormous offset?
If I attach a load which withdraws about 0.3A the raw ADC value is 0x003F, which corresponds to about +1.063A.
If I attach a load which withdraws about 3A the raw ADC value is 0xFF88, which corresponds to about -2.0A. The absolute difference is correct but its normal that its decreasing and having the offset?
Thank you, best regards, Danijel