Hi
I use UCC28220 on the 6KW converter.
Specifications are as below.
-Input: 390V(PFC out)
-Output: 48V 125A(6kw)
Questions
: If you maintain the load, it will work normally, but if you change the load, the MOSFET will die.(ex_ 0A=>20A, 20A=>0A)
I think there is a problem with FEEDBACK. Can you look at the SCH?
The client company can't even reveal the schematic, so I'll send it to you if you know me your email address.
Please let me know if there is anything else to check for review.
Thanks