This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54291: TPS54291 Simulation error

Part Number: TPS54291
Other Parts Discussed in Thread: TPS54292, TPS65270

Hello, 

I have been recently trying to perform simulations on TPS54291 Dual output Buck convertor. I tried simulating in LT Spice and PSpice for TI. Both the time an error appears stating that the "ERROR(ORPSIM-15113): Model MBR330 used by X_U1.D_DRIVER1_D1 is undefined". It seems like the model for the diode is missing. How do I resolve this problem. 

This is the error message from the output window. 

--------------- INFO(ORPROBE-3209): Simulation Profile:  Startup-tran ---------------
INFO(ORPROBE-3183): Simulation running...
** Profile: "Startup-tran"  [ c:\users\acp\desktop\tps54291-pspicefiles\startup\tran.sim ]
Reading and checking circuit
INFO(ORPSIM-15423): Unable to find index file tps54291.ind for library file tps54291.lib.
INFO(ORPSIM-15422): Making new index file tps54291.ind for library file tps54291.lib.
Making index file for library c:\users\acp\desktop\tps54291.lib
Please be patient. This may take several minutes...
WARNING(ORPSIM-15223): Library file C:\SPB_Data\cdssetup\pspTILibDir\nom_pspti.lib has changed since index file nom_pspti.ind was created.
WARNING(ORPSIM-15227): The timestamp changed from Fri Nov  6 12:43:06 2020 to Mon Jan 25 08:48:53 2021.
INFO(ORPSIM-15422): Making new index file nom_pspti.ind for library file nom_pspti.lib.
Making index file for library C:\SPB_Data\cdssetup\pspTILibDir\nom_pspti.lib
Please be patient. This may take several minutes...
ERROR(ORPSIM-15113): Model MBR330 used by X_U1.D_DRIVER1_D1 is undefined
ERROR(ORPSIM-15113): Model MBR330 used by X_U1.D_DRIVER2_D1 is undefined
Circuit has errors ... run aborted
See output file for details
INFO(ORPROBE-3188): Simulation aborted

I need two outputs of 1V and 8V with a current of at least 1.5 or 2A on both outputs. My input voltage is 12V from a AC/DC switching power supply adapter. Are there any better product available to meet my required criterial? I was not able to find a suitable one from TI. Please suggest a solution for the simulation error and if available a suitable alternate IC. 

Thank you. Have a nice day.