This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM41625: Space optimized DC/DC Module Suggestion

Part Number: TPSM41625

Team,

below is the requirement from customer.

The space available for this implementation is only 28x8mm.

What is the best inductor integrated module solution for this req?

Does TPSM41625 meet the space constraint?

Parameter

Min

Typ

Max

Input Voltage

 

5V

 

Input ripple voltage

 

 

10mV

Output Voltage

 

0.8V

 

Output ripple voltage

 

 

10mV

output current

 

 

16.5A