Other Parts Discussed in Thread: ISO7742, ADS7924,
Hi
3 points would like to clarify on this thread
We have 1 ADC (ADS7924), 1 Isolator (ISO7742) & 1 comparator (TLV4082DBV) in our design.
This takes 3.3V and 3mA current altogether.
These devices are powered on the ACFC primary domain (54V and 54V_N).
Instead of using a 54v to 3V3 switching regulator, we would like to source it by one of the below two options
a. from the VREF (5V) voltage of UCC2897A by stepping down it to 3.3V either by diode or resistor divider. would that be feasible?
b. from the bias winding supply (12V to the UCC2897A VDD & PVDD) through a Zener regulator of 3.3V. The bias winding is comfortably can source 30mA as it is designed for max of 170mA
We tried this method but the ACFC generation (20V) is not happening. Any thought on this?
VDD, PVDD current consumption:
The current consumption on the VDD & PVDD is measured as 20mA, when sourced through a 12V bias winding supply.
As per datasheet, load on VDD is very less (around 3mA) and its Vdd voltage range is 8.5 V – 12V – 16 V.
Does the PVDD can take more current in this case? So that we are measuring 20mA.
What would be the maximum supply current for Vdd and Pvdd for our case: Vin = ~ 54V and operating temperature = 0 C to ~ 100 C and XFMR bias voltage = 12 V @ 20 mA?
We would like to source more current from this winding to realize the above mentioned requirement (b) through a Zener regulator (12V to 3.3V with 3mA for circuits).
Regards,
Felix.