This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP87524J-Q1: Disabling FB_B0

Part Number: LP87524J-Q1
Other Parts Discussed in Thread: AWR1843

Hi all,

I am using the LP87524J-Q1 as a power supply for my AWR1843 Board.

We try to operate the system using a Li-Ion Battery (3.2V < VIN_Bx < 4.2V), connected through some protection switch, directly to the VIN_Bx inputs and VANA.

For the System 3.3V we use an independent LDO connected the same way as above (LDO Vin parallel to VIN_Bx).

For such configuration, we don't need the FB_B0 output, in spite of we assembled all its components Lo_0(0.47uHy), Cout_0(22uF), C0(220pF) and R0(3.9 ohm). and VIN_B0 is tied to input voltage (Li-Ion Battery)

My questions are:

1.- Can I remove the above components without affecting the system performance?

2. Can I tie the VIN_B0 to Ground?

3. Can the FB_B0 work unloaded or there is a minimum load I should connect to it? Right now not load at all.

Thanks,

Claudio