Other Parts Discussed in Thread: TLV61048, TPS61170
Hi TIer,
Kindly you help us to suggest suitable converter for following spec, thanks!
Input 12V convert to split positive / negative 15V rail with 50mA.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Unfortunately, we do not have converter that can operate under those conditions. Can you tell me a little bit more about your application requirements? Does it have to be a single with dual output? Or would it be okay to have two devices and one is configured as an inverting?
Thanks,
Alejandro
Hi,
please have a look at this application note https://www.ti.com/lit/an/slvaej3/slvaej3.pdf and select TPS61170 instead of TLV61048