Other Parts Discussed in Thread: BQ21061
Hi All,
I have some question about BQ25155 when I do some battery charger design, as follows:
Q1: Did VDD output can be turned off the output through I2C after the Vin input is disconnected? What is the voltage of VDD at this time?
Q2: CE is the charge enable pin, can i drive it to low all time and don't connect it to host?
Q3: I2C uses the system power supply pull-up design. Whether I2C will stop working when VIN input was disconnected, and will there be leakage at the moment
Q4: Did VIO can be connected to external input directly?
Q5: If LP pin pulled down directly without connecting to the host, did BQ25155 automatically enter low power mode after VIN is disconnected?
Q6: INT is used as an interrupt pin. How many types of interrupts are there?
Q7: If the LDO pin is not used in the design, can it be nc, or the internal can be shut down through I2C. Did LDO still working after vin is disconnected, and what is the leakage current?
Q8: What is the main difference between BQ25155 and BQ21061?
Thanks a lot
Kind Regards